Posted on October 06, 2015 at 13:32Hello all,I'm using two Nucleo-F401RE boards which do some cross communication and timing monitoring. Initally I used boards with revision C-01 and HSI as clock source. This worked fine when doing individual clock-...
Posted on August 21, 2015 at 15:42
Hello all,
When using the STM32CUBEF1 V1.2.0 HAL-library with SPI and DMA transfer just for receiving data, I came across unusual behaviour.
An investigation showed, that the functionHAL_SPI_Receive_D...
Posted on November 06, 2015 at 08:42Hi clive1, thanks for your reply.I see your point regarding HSE / HSI, it definitely makes sense.The issue with the board revision has also been solved, so I'm able to get the new revision from my supplier.Regards...