STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ST-LINK/V2 under Windows 2000

Posted on April 15, 2015 at 21:14Hello, I need to program an STM8AF5289TC using an ICT Tester / Fixture and I just saw that ST-LINK/V2 Works just fine and is small and not expensive for integration, but the problem is that PC controller is Windows 2...

iNemo SWD programming problem

Posted on April 15, 2015 at 19:50Hi to all, I'm trying to program my iNemo based custom board with the ST LINK provided with the STM32F4 Discovery. When I try to connect with STM32 ST-Link Utility I get the error: '' Core is held in reset''. Another...

daniel23 by Associate II
  • 1205 Views
  • 1 replies
  • 0 kudos

ST-Link - Failed to stop the target

Posted on March 26, 2015 at 06:25Hi, I'm using IAR EWARM 7.3. I'm using ST-Link, newest firmware. The target is connected via JTAG. It flashes and seems to run OK - the IWDG is ticking fine without crashing, with RTOS running. I can print using ITM_...

st-link/v2 - Programming Error

Posted on March 02, 2015 at 14:17Hello, i'm trying to load an .hex file into an ARM STM32F103R6 with St-link/V2 but there is something that doesn't work (see attached img). Could you help me pls? #st-link/v2-programming-issue

liberamos by Associate II
  • 5099 Views
  • 4 replies
  • 0 kudos

Unable to program an stm32f030 via st link

Posted on February 19, 2015 at 08:23hello everybody, i am an electrical engineer working with stm32 devices these days. i am having problems at programming stm32f030 via st link utility, i use IAR as an IDE, i have tried hardware troubleshooting, fi...

awais2 by Associate
  • 965 Views
  • 1 replies
  • 0 kudos