cancel
Showing results for 
Search instead for 
Did you mean: 

Cannot connect to target!

jorgentas
Associate
Posted on August 23, 2015 at 14:55

Hello,

First of all i am new to all of this programming.

I am using a St-Link/V2 Isol but everytime i want to connect to the target i get this message

Can not connect to target!

Please select ''Connect Under Reset'' mode from Target->Settings menu and try again.

If you're trying to connect to a low frequency application , please select a lower SWD Frequency mode from Target->Settings menu.

i have connected the board with 

Pin 19: VDD 3.3v

Pin 20:GND

Pin 9:TCK SWCLK

Pin 7: TMS SWIO

they also told me that the ST-Link should be visible as an mass storage on my computer, but it shows up as an usb dongle.

Thanks in advance 

#st-link-utility #no-target-connected
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Posted on August 23, 2015 at 15:46

Suggests the target is non-functional, no details of what it's attached too.

Might want to get Pin 1 connected to the target's voltage.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
jorgentas
Associate
Posted on August 23, 2015 at 17:04

The target is an controller for an E-bike who needs to be reflashed.

http://imgur.com/z1YwePe

________________

Attachments :

Foto_23-08-15_16_40_07.jpg : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HthQ&d=%2Fa%2F0X0000000aVt%2F0tT55uYgprffOVv8HXue0e4VHf.aC3Wv6WdlVZACqQ8&asPdf=false