Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
HelloI'm pretty new to the STM32CubeIDE, and try to flash my test-program (a LED-blink programm) on my NUCLEO-F446RE developementboard. If i press the debug-button, the program is compiled, but then i get the folowing Error:"Error in final launch seq...
Hi I am new in smt32 worldi want to make small project, I want to operate led with USB command through pc with use of stm32f207zct6 micro controller please help me please provide me schematic and code and code for that
We have found that the NRST pin is in Low state after start. This is problem for us because we'd like to use OpenOCD in JTAG mode and OpenOCD will send an active low pulse to NRST pin. Is there any solution for this? Or any other stm32 eval board...
Hi,I have purchased STLink/V3 Set. I was planning to use it together with STM32CubeIDE. Unfortunately, half of the options are working. I quite like it and the speed is similar to my J-Link EDU. SWD/ST Link GDB Server not usable with 24000KHz even on...
Hello,I would like to downgrade STLink V2.I went through this post :https://community.st.com/s/question/0D50X00009XkhxWSAR/downgrade-stlinkv2-firmware-revisionI was able to get some old versions (thanks to contributors) but when I click on "device co...
I want to know if I can use st-link to write code on the stm device^, if not, by which method can I do it?
Installed latest ver STM32CubeIDE in Windows 7Board using stm32f401re nucleoWhen is start debugging I am getting below error “Failed to execute MI commandTarget extended - remote local host 61234Error message from debugger back endLocal host 61234 - ...
Hi,I have a STM32F3discovery board and I just upgrade the STLink Firmware to the last available version V2.J33.S0 (for my board)Does this firmware version supports the Virtual Com Port?I'm not able to see it on my computer, where I already update the...