cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F411RE vs STM32F446RE vs STM32F303RE ?

skrowten_hermit
Associate II

What exactly is the difference between Nucleo boards Nucleo-F303RE, Nucleo-F411RE and Nucleo-F446RE? To me, the data brief seems to suggest that they are the same. Can someone point out the difference? Is it okay if I buy any of these according to the availability? Have attached the Date brief for reference.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Amel NASRI
ST Employee

Hi @skrowten_hermit​ ,

You need to refer to UM1724.

-Amel

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

4 REPLIES 4

FLASH, RAM and SPEED?

F3 has different ADC performance.

You should probably look up the webpages for the micro-controller placed on each board.

If all that is unimportant for your unspecified application, any of them would suffice.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
Bill Dempsey
Senior

As stated above, there are speed & core ram/flash differences but also additional/different peripherals: CAN, UARTS, I2S, SPI (count), USB (type), etc...

There are nice pictorials of the boards over on the mbed.org website (color breakout of features on board) that might make it easier to understand

https://os.mbed.com/platforms/ST-Nucleo-F446RE/

https://os.mbed.com/platforms/ST-Nucleo-F303RE/

https://os.mbed.com/platforms/ST-Nucleo-F411RE/

This helps. I was looking for something like this. Thank you!

Amel NASRI
ST Employee

Hi @skrowten_hermit​ ,

You need to refer to UM1724.

-Amel

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.