Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Such an equipment is literally nowhere to be find, could You help me find required adapter and cable? I'm sending photos, hope it helps.
Hi I installed STM32CubeIDE V1.1.0 and now I can't select J-Link as a debug probe, only ST-link (GDB & OpenOCD).I get the J-link if the project was created in an older STM32CubeIDE version, but not in the new 1.1.0.Any hints on how to enable J-link?
My NUCLEO-G841RB USB plug into the computer does not recognize the driver. My operating system is WIN7 64bit. See the figure below for the driving situation. keil is uvision5.28.0.0.
Hello everyone!We are using the STM32F103RBT6 and able to program our devices using the ST-LINK / V2. Usually not a problem but recently we have had one device that after programming successfully, verified and checksum showing correctly there is an e...
Hello There,I dont know if this is the right place to get help. I am a newby and working with STM32H747I DISCO.Currently ST-LINK cannot connect my device. I did the following troubleshoot based on online solution.==> Update stlink utility==> Pull boo...
Has anyone been successful in enabling and using dual-core debugging of this H745I-DISCO board using the on-board ST-LINK v3 interface? I am able to use the interface to dowwnload and debug each core separately; however, I can't get the ST-LINK sh...
issue-when programming using the Command line utility it indicates success but the unit does not boot. when programming from the GUI the unit powers up correctly. I used the same command line on an st32f07 without issue. Here is the command line....
HelloI'm developing an application with an STM32F750Z8 and I need to put the code in the external flash and then debug it. I tried to implement the firmware:1) I created the Launcher with STMCubeIDE and STMCubeMX and programmed the microcontroller wi...
HiI am starting to develop a new project using the STM32F469I-Discovery Board using the TouchGfx library.I am using the CubeIDE (v1.1.0) and trying to use the ST-Link GDB Server for debugging. The ST-Link is taking a very long time to download a new...
I'm trying to get myself situated to program comfortably with my STM32 Blue Pill and STLink V2 USB interface. However, I've run into an issue when trying to gain access to the VCP (Virtual COM Port) that the STLink is supposed to open up for me when ...