cancel
Showing results for 
Search instead for 
Did you mean: 

How can I set the frequency for GDB-server from STM32CubeIDE in order to debug STM32F105 target.

JStep.1299
Associate

I can connect from STM32CubeProgrammer via ST-Link/v2 running V2J3457 when I lower the frequency from 9000Hz to 2250Hz. However, I can't connect from the STM32CubeIDE debug because there is no (obvious) way to set the frequency.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Markus GIRDLAND
ST Employee

You'll need to start it as "stand-alone" and pass the frequency as an argument, you can read more about it right here.

View solution in original post

1 REPLY 1
Markus GIRDLAND
ST Employee

You'll need to start it as "stand-alone" and pass the frequency as an argument, you can read more about it right here.