STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! No device found on target. ?

Hello,After copying an STM32CubeIDe project using the New → Project from .ioc file and then importing old project version into the one, the IDE wont let me program the device.With old project version, I can run the programming Run settings and the ST...

simo zz by Senior II
  • 1241 Views
  • 1 replies
  • 0 kudos

Unable to upgrade STlink on Dev board

Nucleo-H743ZI2 Dev BoardSTM32CubePRogreammer V2.3, and V2.4OS: Windows 10 Using CubeIDE with a new board I get the popup saying that the board needs an update. The IDE was unable to successfully do this. So I attempted CubeProgrammer 2.3 with no luck...

PLane.1 by Associate II
  • 2492 Views
  • 3 replies
  • 0 kudos

Resolved! STM32CubeProgrammer works fine with NUCLEO STM32F767ZI but fails to find NUCLEO STM32F446RE.

Hi, I have 2 Nucleo boards: NUCLEO STM32F767ZI (F4) and NUCLEO STM32F446RE (F7).I'm using macOS 10.15.4 omn MacBook Pro 2017 with STM32CubeProgrammer 2.4.0 and stlink tools from brew (GitHub.com/texane/stlib).When I plug in F4 over USB-C to USB-Mini ...

kj.obara by Associate III
  • 1779 Views
  • 6 replies
  • 0 kudos