cancel
Showing results for 
Search instead for 
Did you mean: 

STLINKV3 Mini CN3 and Reset usage

raptorhal2
Lead

On the STLINKV3 Mini, what is CN3 used for and what are the signals?

Do the two reset pins have a useful user function?

No information on this is available in the current user manual.

Cheers, Hal

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Uwe Bonnes
Chief

CN3 is probably the SWD connector used for initial device programming. Have a look at the Nucleo-G47 schematics CN2.

raptorhal2
Lead

Thank You.

No room to say "Reserved" on the Mini.

The Reset pins probably also have a manufacturing only purpose.

Cheers, Hal