STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STLINK Cannot Detect Target Voltage

I am using an STLINK V3SET and the STLink Utility v4.5.0.0. I have opened up the V3SET and I am measuring at the pins of the connector to the target the correct 3.3V between pins 3 and 5 as indicated in the user manual. This voltage is coming from th...

WTetl.1 by Associate
  • 1427 Views
  • 1 replies
  • 0 kudos

Resolved! ST-Link V2, device not found error.

Hello. I just got a ST-Link V2 and wasn't able to program/debug a STM32 MCU with it. With a fake programmer I can program succesfully. But when I try to use ST-Link V2, it gives me device not found error. I wire STDIO, SWDCLK and GND pins to the targ...

GunkutA by Senior
  • 1402 Views
  • 2 replies
  • 0 kudos

Resolved! STLINK V3 CubeIDE

Hello;Can anyone run STLINK V3 with CubeIDE? I can delete and load the hex code inside the processor using STLINK_Cube Programmer.But when I try to enter debug through CubeIDE, I get the following error. Anyone who has encountered this error and can ...

0693W000001qqc5QAA.png

I am looking for some more information relating to power requirements of the STM32F413 which I am designing into a system. (STM32F413ZHJ6)

I need additional information on the IC characteristics in order to run accurate power integrity simulations in Hyperlynx. The IBIS model supplied does not take package characteristics into account. In addition to this, there is the internal regulato...

NMcGi.2 by Associate
  • 573 Views
  • 0 replies
  • 0 kudos

ST-Link Upgrade window no show

When the stm42f429-discovery board was connected to my MacBook Pro 2019, I clicked the ST-Link Upgrade from Help pull down manual, no window popped up. But when I run the debug of the demo project, IDE was able to find the board and run the demo proj...

DZhan.1 by Associate
  • 738 Views
  • 0 replies
  • 0 kudos