STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I wanted to order an cortex M7 mcu,I currently using an stm32f1 series with stlink v2 clone.My problem is that im not sure which debugger/programmer should i order for cortex M7 series? .Also whats the difference between STLINK-V3MINI and STLINK-V3MOD

I read the manual and its says " The STLINK-V3MINI embeds an STM32 32-bit microcontroller based on the Arm®(a)Cortex®-M processor " same fore the VMOD but i wanted to reassure that im getting the right debugger/programmer?

Oahme.1 by Associate III
  • 3036 Views
  • 7 replies
  • 0 kudos

Missing labels on STM32H750B-DK schematic

Hello -The schematics posted on the website for the STM32H750B-DK board do not have any of the off-sheet or power ports labeled. This makes it impossible to follow the power connections on this schematic:https://www.st.com/en/evaluation-tools/stm32h7...

KMurp.290 by Associate II
  • 1172 Views
  • 2 replies
  • 0 kudos

Any new Nucleo boards this year?

Hi everyone, I just wondered if anyone is privy to information if STMicroelectronics is still in the maker business, that is do they plan any new Nucleo boards for hobbyists this year? Or maybe that was too much hassle for the company and not worth i...

kj.obara by Associate III
  • 1580 Views
  • 3 replies
  • 1 kudos

Resolved! Hi, I can't connect to STM32F030R8T6 using ST-LINK V2 and STM32CubeIDE on Ubuntu 18.04.5 LTS.

I use STM32F030R8T6 and an interface card that plugs into a breadboard for direct prototyping, ST-Link v2 STM32 and STM8 Programmer, both from Newbiehack.com.Connected as on photo: SWDIO to pin 46 (PA13), SWCLK to pin 49 (PA14), GND to pin 62, 3.3V t...

Adam_K by Associate II
  • 12961 Views
  • 6 replies
  • 0 kudos

Is there a way to power a nucleo 64 board from a 3V external battery without damaging the board?

Hello,I'd like to power my nucleo L152RE from a 3V external battery.I thought this should be easy but then I read that some soldering needed to be done? Is that true? I'd like to be able to power the board from an external 3V battery to use it as an ...

BCora.1 by Associate III
  • 4315 Views
  • 7 replies
  • 0 kudos