User Activity

Hello, everyone. I need to generate a stable 12V to supply my cooling fan (current consumption not over 200-300mA). The input voltage is in the range of 10V to 26V. Consequently, some buck/boost topology will be needed. I came across the MCP34063 mod...
Hello guys, We should start soon with the development of our new version of an IoT board that is controlled through the Google Cloud IoT by the help of Ethernet connection. We have a goal to replace ESP-32 module we are currently using. In that sense...
Hello guys. As indicated in the title, I have an STM32H7B3I-DK board here with me. I am trying to play with it but currently having a hard time to load the code to the board from Keil MDK v5.23. When I compile the project and press a Download button,...
Hello, guys. I recently bought STM32H7B3I-DK and started playing with it. There are a few questions/issues I have:1) It seems that the board is recognized by the host PC only when it is directly connected to the PC's USB port. If I connect it through...