STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Did I destroy my STM32F7? (SB12 removal)

Dev board: Nucleo-F767ZIDear all,as I wanted to have my own Vref+ for ADC conversions I removed solder bridge SB12 (coupling Vref+ with VDD) to input my own reference voltage (~3V) at Pin 6 CN7.After removing the SB12 however the STM 32 device is not...

0693W00000Bc6XQQAZ.jpg
AKuts.1 by Associate
  • 2578 Views
  • 3 replies
  • 0 kudos

Updating the firmware of a X-NUCLEO-BNRG2A1 using the integrated ST-LINK V2-1 of a NUCLEO-L476RG

I'm having trouble updating the firmware of a X-NUCLEO-BNRG2A1 using the procedure described in AN5651 page 4 ("Direct update on the X-NUCLEO-BNRG2A1 expansion board" through the NUCLEO64-L476RG integrated ST-LINK 2-1).I get this error message in FAI...

paul19 by Associate III
  • 2123 Views
  • 3 replies
  • 2 kudos

Resolved! ST-LINK error after Firmware update

Hi,I connected my brand new STM32F769I EVAL board to power and to PC through USB ST-Link port, I opened STM32CubeProgrammer, picked ST-LINK connection on the top right, clicked Connect, and it said that I need to perform a firmware update first. So I...

Alaa by Associate II
  • 4916 Views
  • 1 replies
  • 0 kudos

ST Link CLI

I am using the ST-Link CLI tool in windows.I am able to progam a virgin unit and after a power cycle the correct software is runningHowever a need to make a testjig setup. The unit is powered by USB so after programming I need to reset the unit to ru...

LHoug.1 by Associate II
  • 1755 Views
  • 2 replies
  • 0 kudos

Resolved! STM32L4P5 cant run after loading SW. The SW runs on Nucleo board well and as soon as I load the file to the custome board ....I manage to identify the chip and load the FW but STM doesnt run

I am using KIEL with ST-LINK V2 programmer Boot0 ( Pin number 138) tied to LOW via 10K resistornRST has a 100nF to GND and a pull up resistor 10KChecked the POR and it looks fine It looks like the chip doesnt run Please advise

MTzie.1 by Associate II
  • 1584 Views
  • 2 replies
  • 0 kudos

Resolved! STM32F746G-DISCO, STM32 ST-LINK Utility

STM32 STLINK Utility has stopped working. I'm sending the setting. What could be the reason?[Settings] File= address=0x08000000 size=0x1000 data_width=4 connection=SWD SwclkFrequency=15K freq=8000 Connection_Mode=Normal DebugInSleepMode=1 Reset_Mode=...