STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32L562E-DK board current consumption

Hello everybody,I am developing an embedded application using STM32L562E-DK which autonomy has to be greater than 3 months.My problem is that I remarked that the board consumption (not including the MCU and its peripherals) is about 120 mA. I precise...

ABois.11 by Associate II
  • 1574 Views
  • 4 replies
  • 0 kudos

V2.J27.S6 Firmware

I have an ST-LINK / V2 Programmer with the number B 2018 33 containing Firmware V2.J27.S6, we are completely satisfied with it. The service needs in the field forced us to buy another ST-LINK / V2 with the number A2021 03 containing Firmware V2.28.S7...

SSzub.1 by Associate
  • 1709 Views
  • 3 replies
  • 0 kudos

Can't connect to STM32H7 board

I've been working with the STM32H7B3LIH6Q board on Segger, and it was functioning normally until I happened to flash the code below to it. Now I get "no idcode detected" on Segger and "No debug probe detected" on STM32CubeProgrammer when connected to...

FSkro.1 by Associate II
  • 1679 Views
  • 1 replies
  • 0 kudos

STM32F429B JTAG Works, SWD not!

Hello dear engineers,I have made a custom header board based on the STM32f429BIT6. The board can be programmed with the JTAG interface. AS SWD and JTAG share the same connection, (JTAG needs more connection), I assumed that it would be possible to ch...

STM32L4R5ZI USB Hardware Design

Hi, I'm trying to design the USB OTG function on my PCB with STM32L4R5ZI. I saw the training documents and video on ST website and I'm confused about how to connect the TVS diode. There's a youtube video as well. Since I'm using the OTG function, it...

0693W00000BZXwWQAX.png 0693W00000BZXx5QAH.png
CYeow.1 by Associate II
  • 1371 Views
  • 1 replies
  • 0 kudos