Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
I join the schematic of my board to the question. I am unable to connect my custom board, the error message on STM32CubeProgrammer is "Not STM32 target found" even it detects the supply voltage. The VDD required for the MCU is 1.8V and I connect all ...
I am in the process of designing a new controller for a product and the only processors that seem available in any quantity are the -P versions. The datasheet isn't clear for these if the SMPS is optional and you can just use the internal LDO, or if ...
"ST-LINK/v2"�?�該�?�判定書を頂�?�る�?��?�ょ�?��?�。購入元�?�廃業�?��?��?�り�?該�?�判定書�?�発行�?�出�?��?�困�?��?��?�り�?��?�。よ�?�?��??�?�願�?��?��?��?��?��?�。
Hi, I've come across a few of these issues namely here but I haven't found a fix for my issue yet. I have a custom PCB based on the STM32H745ZIT6 chip which I wired up to be powered using the LDO power supply. However, I'm running into two problems a...
Hello,As the questions says, I'm having difficulty programming a Nucleo-F334R8 board directly via the PA13 and PA14 SWD pins. After removing the jumpers on the built-in ST-link (CN2) I have connected the external ST link directly to the SWD, reset, g...
I have ST-LINK V2 Programmer and when I connect this with STM32MCU, it shows an error like this I have checked connections, jumper Wire.Changed the port also. But still, it is showing No STM32 Target Found. For checking Whether My Programmer is corru...
On Nucleo H753ZI normally PG7 is used as USB FS overcurrent indication input and has a red LED on it.I need PG7 as output (don't ask why) going to external connector. Not using the USB FS function.So when PG7 is set low, the overcurrent LED glows.Can...
Hello,I have an issue with the Nucleo-G474RE, I can't get the JTAG to work, I tried JTAG in 4-pin and 5-Pin-Mode, the IDE reports "No device found on target". With SWD it works in ST-Link-GDB-Server-Mode, but not JTAG. I checked JTAG is connected to ...