Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Hello, I have a STM32F407VGT6 built into our application, During developement Iam facing some strange issue where NRST pin goes below logic level over the time(in few days), This issue happens in some of our boards. Our Circuitary only contains 0.1uF...
Hi,I'm working on a STM32F7508-DK recently bought. I've imported an example project from stm32f7 packages called Menu_Launcher. I'm trying to run the project with OpenOCD but this doesn't work and I have the following errors in the console :Info : Li...
Dear Master,I have problem dealing with STM32L4Q5CGT6, i just turn on the peripheral like SPI, I2C, UART and set the core clock to 400KHz.in the datasheet and PCC says the current consumption (IDD) will be around 300uA.but in actual i measure the idd...
Hello,This is my first time designing a PCB for an STM32F4 microcontroller (and I only get one shot at making this board), and the specific application requires USB and a CAN-Bus. I chose a 10 MHz through-hole crystal oscillator (ABL-10.000MHz-B1U-T)...
I've designed a board that uses an STM32G030F6 processor. Now I've updated the software and... (one feature wasn't implemented yet) I cannot connect to the target CPU to flash tne new firmware into the board. Then you'd think I've programmed the SWD ...
Hello community,I'm designing a schematic which involves a STM32L476ZGT6.I'd like to know if a document of design recommandation exists else than the document "AN4978 Application note. Design recommendations for STM32L4xxxx with external SMPS,for ult...
Just bought a nucleo H745ZI-Q board and trying to use the debugger. I'm using the STM32CubeIDE and the program exits with the error 'Info : stlinkserver already running, exit'I'm just hitting 'debug as' in the run menu and selecting my device. The ac...