STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32F4 Discovery : Why U4A and U4B in schematics when the MCU is marked as U4 on the PCB?

I'm just learning to read and use schematics and I found that while physically the MCU (STM32F407VG on my STM32F4 Discovery board) is marked U4 as the part number on the PCB, the schematic (Section "STM32Fx" of "MB997-F407VGT6-D01_Schematic.pdf") sho...

0693W00000FCwrqQAD.png

GPIOA interrupts not arriving when Nucleo F446RE is on external power and ST-LINK is disconnected, GPIOC interrupts arrive fine

Hi,In my application running on a Nucleo F446RE I notice that EXTI interrupts from GPIOA are not arriving in the EXTI15_10_IRQHandler() when the Nucleo board is connected to external power on E5V, JP5 on E5V and the ST-LINK is disconnected from USB. ...

Kvan .7 by Associate II
  • 4682 Views
  • 6 replies
  • 0 kudos

Which is the best stm32 board (nucleo or evaluation) with embedded high performance DAC for sinusoidal signal generation? see next details.

I am looking for a microcontroller board for the following application:Receive a square wave LVDS signal at 1 kHz (more or less) and generate 2 sinusoidal single-ended output with the same frequency of the incoming square wave with the highest resolu...

Tommino by Senior
  • 3428 Views
  • 4 replies
  • 0 kudos

STM32F407VGT6 NRST pin going Low

Hello, I have a STM32F407VGT6 built into our application, During developement Iam facing some strange issue where NRST pin goes below logic level over the time(in few days), This issue happens in some of our boards. Our Circuitary only contains 0.1uF...

Vb.21 by Associate II
  • 5692 Views
  • 9 replies
  • 0 kudos