Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Can anyone help me to handle with a openocd issue? I got a message as follow "Failt to launch OpenOCD GDB server:timeout" in VSC. The output message are Info : Unable to match requested speed 1000 kHz, using 950 kHz Info : Unable to match requested s...
I got stm32l476g discovery kit.but I never found schemetic for stm32l476g discovery kit in "st.com"How can I find schemetic for stm32l476g discovery kit?
If I remove the SMT32L476RGT6U IC on the Nucleo L476 board.I will mount the SMT32L476RGT6U IC on an external PCB.Now, I will connect the required pins of IC with CN4 of the Nucleo Board.Is it possible for debugging for external application? My inte...
Hello, I am struggling finding electrical peripherals interconnection information for STM32F469. Peripherals are not covered in the datasheet, and I have looked thru Application Notes to best of my ability. Is there a document I missed that goes over...
This question pertains to an STM32F413 target board I constructed.I deliberately skinnied down my target's programing port to include only these barebones signals mentioned in the STLINK V3SET user manual: T_VCCT_SWCLKGNDT_SWDIOT_NRSTT_VCP_TXT_V...
Hi,I'm mounting STM32L476RGT6U on PCB. For that, I have made this schematic. I need some expert suggestions from anyone who has in-depth knowledge of this. I'll use an ST-LINK V2 to debug and upload the program to the MCU on PCB.
MCU is STM32L0.The file I use to program has option bytes added with read-protection turned ON. :020000041FF8E3 :0C0000000000FFFF7A80857FFF0000FFFA :00000001FFUsing ST-link V3, I'm having this error: (see attached screenshot) Command line:stm32_prog...
As above, have a project I'm porting from one custom board to another. Using the same external crystal (8Mhz) and virtually identical circuitry with the exception of a few custom ASICs. This code works fine on the L432, but when I run it on the L496...