STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Digital inputs in STM32 boards ?

I am working on reading an External 3 bit parallel CMOS ADC (4-8 MSPS)(from MAX2771 board or Eva KIT) GNSS digital output. I want to read this digital output pins using the NUCLEO-H723ZG, I do not know if there is digital inputs pin in the board ?if ...

AElta.1 by Associate II
  • 2146 Views
  • 2 replies
  • 0 kudos

Failed to start GDB server Error in initializing ST-LINK device. Reason: (4) No device found on target.

Hello, I am using an STM32G031 Nucleo 32 board. Everything worked well. Following break point I lost the gdb server connection. Unable to reconnect, I made an update of the driver st link. I started under reset, reinstalled an old st link driver... I...

0693W00000NrCrUQAV.png

Resolved! ST-Link/V2 cannot detect STM32 target

I have bought a new ST-Link/V2 from Digikey a while back and have only recently gotten the chance to use it. But every time I try uploading code to my geniune WeAct F411CEU6 board using SWD I get the error code "Error: No STM32 target found!". I don...

JTurn.2 by Senior
  • 12812 Views
  • 10 replies
  • 0 kudos

Resolved! Extremely high current draw in L031K6T7

I'm running into an issue while designing a relatively simple custom board with an L031K6T7, where after programming it the current draw exceeds 200mA and eventually breaks to the current limit of the power supply at 800mA.When I assemble the board t...

Alec1 by Associate II
  • 14071 Views
  • 10 replies
  • 1 kudos

Resolved! USB-UART stability issues over STLINK when "Mass Storage" type enabled on MACOS

I've found that Nucleo-L4R5ZI and Nucleo-L476RG sometimes stop receiving UART data through the STLINK USB interface is Mass Storage type is enabled.I created a program that echos random data sizes (send to board, board echos back). This will crash af...