STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ST-link driver

I have stm32F407 discovery board and I have downloaded and installed the ST_LINK USB driver on my laptop running window 10, but when I plug in the discovery board, the error message pops up saying the USB driver is not recognized, in the device manag...

0693W00000NrxeXQAR.png 0693W00000Nrxf1QAB.png
lzhan.21 by Associate II
  • 2084 Views
  • 4 replies
  • 0 kudos

Reset of the controller

Very new to ST and struggling to understand the basics. As posted in previous posts i am using the STSPIN3201 motor controller, i am trying to write the basic LED toggling program. From STSPIN32F0 data sheet i found the micro used is STM32F031C6. I c...

0693W00000NrRvqQAF.jpg 0693W00000NrRw5QAF.jpg 0693W00000NrRwFQAV.jpg
JDesi.1 by Associate II
  • 7510 Views
  • 11 replies
  • 0 kudos

STM32F407VET6 heats up

Hello!Yesterday I was using somesensor with the STM32, and today I realized that the STM32 and the voltage regulator heats up. Also my two alternative STlink connects and disconnects from the USB. I uploaded an empty project, but it still the same. U...

SGonz.2 by Associate II
  • 2004 Views
  • 2 replies
  • 0 kudos

Resolved! How to write plain intel hex to flash?

Hi,I would like to copy the exact contents of a hex file to the flash memory of my f446 nucleo, complete with byte count, address info ....Is there any way to do this? Using ST-Link I can only find options to actually flash the hex file or manually a...

gfxfloro by Senior
  • 11908 Views
  • 21 replies
  • 0 kudos