STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Which software to be used when using Nucleo board as a debugger to an external board as SWD?

I want the Nucleo board 303RE to act as a debugger for my external board. Two boards have an individual 3.3V supply so the ground has been made common. Other Hardware connections are below. Since CUBE IDE doesn't allow to flash Bin files using ST-LI...

0693W00000NsX04QAF.jpg
RAnan.3 by Associate III
  • 2606 Views
  • 6 replies
  • 0 kudos

I have a question regarding the STM32L083CZT6 microcontroller. I have designed a custom board using this microcontroller, but it's not working!! Do you have any tips?

I have tested the microcontroller with different boards and all have the same problem. I have noticed that the voltage across the NRST is 0V, which I think means that the microcontroller is damaged (There is no short circuit in the system). I have co...

0693W00000NsUPVQA3.jpg
AHamz.2 by Associate II
  • 7145 Views
  • 23 replies
  • 0 kudos

Resolved! Pinouts: STM32F429IGT6 to B-U585I-IOT02A

I'm looking to connect a Waveshare e-Paper display to my STM32U5 discovery kit (B-U585I-IOT02A).On the Waveshare website (https://www.waveshare.com/wiki/7.8inch_e-Paper_HAT), they have a pinout for the SPI bus on a STM32F4 chip as follows:Connect to ...

VLaPo.1 by Associate
  • 2631 Views
  • 2 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.