Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Title edited to reflect that this relates specifically to the NUCLEO-G070RB board.NUCLEO-G070RB in this board ADC channel 0,1 working ,other ADC channel not working is they any reason?
Dear ST Technical Support Team,I am writing to request technical assistance regarding a recurring hardware failure with the STM32H743IIT6 MCU on my custom-designed PCB.Problem Description:After initial assembly, the MCU is correctly recognized by STM...
Hello all! I need some rubber ducking help here. I have got hold of a B-U585I-IOT02A dev board, where I'm trying to get learn and get to know the STM32 family. I have got a lot of things working, but the ADC1 is giving me a hard time: Here is my MX c...
Hi,I want to create a pin-compatible board to X-NUCLEO-SRC1M1 to further explore USB-C charging, is there a STEP or DXF file available for this or any other X-NUCLEO board that has both the ST Morpho and Arduino UNO R3 connectors please?Kind regards,...
Split from Transmit line stuck high on STM32F415 with MAX3232 - this is a new questionWhat ST board would you recommend? This is not really my realm. Thanks!
Is there any utility in the holes and silkscreen circles around the TFBGA225 on the NUCLEO-H7S3L8? It appears to be the same pattern on the Discovery board, suggesting it might be for BGA placement or maybe a heatsink. Edited to put the image in-lin...
Hello, I am using an **STM32 NUCLEO-N657X0-Q** board with the **B-CAMS-IMX camera module**. Originally, the board was working correctly. In **DEV BOOT mode**, I loaded and ran my AI model, using the B-CAMS-IMX camera sold by ST. The board connected n...
Hi, On STM32F746G-DISCO board I have a problem with USART1 (ST-Link VCP): - TX (PA9) works fine – I can send messages- RX (PB7) doesn't receive any characters and I think the board is not waiting for commands Tested both polling (HAL_UART_Receive) an...
Is there a prize for the most trivial post? Opened up a new Nucleo-L476RG board (finally worked my way through the 10+ boards I bought a number of years ago) - it comes in a cardboard box now, nice. The Leds (LD1, LD3) were so bright, I couldn't prob...
I'm back, and working with the stm32g070rb chip. I did prototyping on a nucleo board based on the same chip (split the st link and nucleo board), and wired the ST Link to the microcontroller with the following connections I used open-ocd for flashin...