Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Dear Sir.Attached a code of SystemClock_Config();void SystemClock_Config(void) { RCC_OscInitTypeDef RCC_OscInitStruct = {0}; RCC_ClkInitTypeDef RCC_ClkInitStruct = {0}; /** Configure the main internal regulator output voltage */ if (...
I created PCB by basically following this design, but I used as MCU the STM32F303CBT6. Programming through FTDI programmer works all fine, but when I try to use the onboard USB port, Windows doesn't want to accept it and in device manager says that i...
I started from the documentation of both discovery board and MB1280-B1 STMOD board.They both state, that the pin number 2 of STMOD+ (P2) connector of the discovery board is connected, I quote: "SPI2_MOSI/ USART2_TX (PC3/PD5)".So - USART2, pin PD5. Th...
I am using STM32CubeIDE for my project . when i want to run the code i am getting this pop up.i am not able to solve this issue.
Hello, I am working on the project from scratch. I would like to know what are the minimum connections I will need for the STM32F429VIT6 in order to program? I have segger J-Link which I will be using. so far I have connect SWCLK (Pin 76), SWDIO (Pin...
Or do I need to fit them to my board?
I'm running a STM32L496ZGT6U on a NUCLEO-L496ZG. Previously, I used the NUCLEO's integrated ST-LINK/V2-1 debugger/programmer. Now, I have sawed off the ST-LINK part of the PCB. I want to program and debug using a STLINK-V3MINI. I wired up STDC14 for...
In UM2179 Rev 9 it says:"5.4.4 Using ST-LINK/V2-1 to program and debug an external STM32 application...Note:JP4 NRST (target STM32 RESET) must be open when CN3 pin 5 is used in an external application."This is CN3: I think that should be CN5.
I am running Kiel uVision under the free LO licence and I can program the board and read it back in ST-Link V2 so i know I have connections to the device, however whenever I try and connect to the device to debug I get an error "Cannot access target....
I purchased a new ST-LINK V2 ISOL debugger but whenever i connect it to my custom STSPIN32F0 board using SWD protocol (VCC, SDA,SCLK, GND), its showing no STM32 target found and error showing target voltage is too low but 3.3 V showing on the VCC pin...