STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Hi, I could not get st-link/v3 mine and stlink-v3set connected to STM23l152C6T6. But all works fine with st-link v2. Any idea ?

Issues confirmed on Win7 x64 and Win10 x64, STM32CubeProgrammer v2.12.0 was used on both platforms.Both v3 versions working fine with STM32F103ZE, STM32F103ZG, STM32F103RC, STM32F103RE, STM32F103RD configurations as v2 does.I read advises to reduce ...

DLyas.2 by Associate II
  • 2608 Views
  • 4 replies
  • 0 kudos

Resolved! 32F413: Strange VCAP1/VCAP2 Behavior?

I'm debugging a hand-stuffed PCB that could have a component stuffing error I cannot discern. The board's artwork is a minor tweak on a prior known-good PCB using a 32F413 in the 100-pin package.This board will not boot.However, all VDD pins are at ...

JOLSO.11 by Associate II
  • 1903 Views
  • 2 replies
  • 0 kudos

Cannot acces to COM port while debugging

Hello,I'm working on STM32CubeIDE with STM32F103CF8T6 and st-link.I have a python script on my computer sending data to the stm32 trough com port. Everythings works fine when I run it, but when I run it in debug mode, I cannot acces to the com port a...

DHorn.3 by Associate
  • 1845 Views
  • 2 replies
  • 0 kudos

I have STM32H7A3ZITXQ_RAM.ld in NUCLEO-STM32H7A3 Board. I need to know what is the procedure to download and run project from Internal SRAM of STM32H7A3 Nucleo(144)Board.

I have STM32H7A3ZITXQ_RAM.ld in NUCLEO-STM32H7A3 Board.I need to know what is the procedure to download and run project from Internal SRAM completely of STM32H7A3 Nucleo(144)Board.I built Base Default Nucleo-H7A3 STM32 Board .ioc Project in STM32Cub...

AR.11 by Associate
  • 1157 Views
  • 1 replies
  • 0 kudos