STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

I have some problem with stm32h723zg uart

I was working with stm32h723zg uart3 pin. I was using micro usb pin with stlink for uart and It works fine but I relise I have to use 3.3V power for pwr consumption test with stlink-v3pwr so I set jp2 with no jumper, and set on jp1 which it will set ...

MChan.12 by Associate
  • 1204 Views
  • 0 replies
  • 0 kudos

St-link v2 upgrade to 3.11.3 seems to cause a "target no device found" problem. I was wondering if this is due to me using el cheapo generic stm32f401cdu6 boards? Is there chip counterfeiting happening, and has ST started testing for counterfeit chips?

This problem exists with both a nucleo 446re programmer as well as multiple generic stlink v2 programmers. These programmers will all update successfully from the stm32cubeide. I have tried different debugger settings. This "target no device found" ...

SJone.4 by Associate
  • 1167 Views
  • 1 replies
  • 0 kudos