2022-06-07 5:33 AM
I would like to know if the micro can work exclusively with the internal LDO for the Vcore
Solved! Go to Solution.
2022-06-07 6:56 AM
Welcome, @ILobo.1, to the community!
The external SMPS is intended exclusively for the possibility of maximum energy saving if you supply the STM32 e.g. via a battery or from an energy harvester.
Of course, you can use the STM32L496 without an external SMPS and only with an internal LDO, but then you will burn up considerably more electrical energy, as you can see from the corresponding parameters in the data sheet.
Does it answer your question?
Regards
/Peter
2022-06-07 6:56 AM
Welcome, @ILobo.1, to the community!
The external SMPS is intended exclusively for the possibility of maximum energy saving if you supply the STM32 e.g. via a battery or from an energy harvester.
Of course, you can use the STM32L496 without an external SMPS and only with an internal LDO, but then you will burn up considerably more electrical energy, as you can see from the corresponding parameters in the data sheet.
Does it answer your question?
Regards
/Peter
2022-06-09 1:48 AM
2022-06-09 5:23 AM
Great!
If the problem is resolved, please mark this topic as answered by selecting Select as best. This will help other users find that answer faster.
/Peter