STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H747i-Disco LCD Driver Issue

I have been working with the STM32747i-Disco and the STM32F769--Disco boards. Both have the MB1166-A09 LCD daughter board attached. I have implemented the LCD_DSI_CmdMode_DoubleBuffer example for both. Teh H747 platform took a little more work as the...

SLimi.1 by Associate III
  • 2875 Views
  • 1 replies
  • 0 kudos

Resolved! GPIO outputs are in high-impedance state

I have two of the STM32H747I-DISCO boards. I have used STM32CubeIDE to create a simple project for the boards. I followed AN5361 and am able to debug and see the CM7 and CM4 cores running.I've added code to toggle the board LEDs (port I) but don't se...

Resolved! I2C Data Transfer Problem

I am trying to send data over I2C3 Using STM32F429 Dev Board and Everyting works fine except the HEX Data I want to sendI am Passing this function HAL_I2C_Mem_Write(&hi2c3,0x30<<1,0x09,I2C_MEMADD_SIZE_8BIT,0XFF,1,100); And Getting the Following Outpu...

ZExpo.1 by Senior
  • 2045 Views
  • 2 replies
  • 5 kudos

Resolved! STM32H747-DISCO cannot run at 480MHz

Hi,I have bought the STM32H747-DISCO kit for testing and I want to test at the max frequency (480MHz). I'm aware of the requirements for the 480MHz, I have followed the user manual:Desoldered and soldered relevant SBs for LDO operation.Updated the co...

filipxsikora_0-1694806637950.png

Microphone and Codec

Hi,I have a STM32F407G-DISC1 board and would like to use the on-board microphone to collect audio and send it to the on-board codec and listen to the collected audio on earbuds. Is there any example on how to do this?Thanks!

CWang.2 by Associate II
  • 2544 Views
  • 3 replies
  • 0 kudos