STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Buttons for sending Can Frame

Hello . I need to send 6 different 8-bit frames via Can to an external device using buttons. I will connect either 6 buttons to the GPIO inputs to stm32f407. 1 frame 8 bit. How to do it. Could someone help me with this?  It's about adding buttons to ...

Siwyzg by Associate
  • 1345 Views
  • 1 replies
  • 1 kudos

Resolved! External Powering of Nucleo Boards

Hello, I am not experience enough in electronics to know if this is a dumb question but I'd like to know what the max current of the NUCLEO boards means. Is it the maximum current draw or the limit that is input from the output source? I'm wanting to...

STM32L496ZGT6P doesn't power on

I assembled 2 boards (my design) with STM32L496ZGT6P.I loaded the firmware..OK The first board works fine The second board sometimes doesn't power on. I checked the voltage (VDD).... is correct, but the microprocessor doesn't power on. It's a *** pro...