cancel
Showing results for 
Search instead for 
Did you mean: 

Change OSC_IN pin with OSC32_IN ?

hazall
Associate III

I am using STM32F030C8T6TR. An external 8 mhz oscillator was connected to the OSC_32_IN-OUT input by mistake, not to the OSC_IN-OUT pins on the board I have. Hardware cannot be changed. Can I reconfigure the pin with software or How can I use it? I am new in stm32.

Thanks from now :)

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Peter BENSCH
ST Employee

The oscillator pins are fixed and not interchangeable. Only the GPIO alternative can be selected. In this respect, you will have to make a new layout.

Hope that helps?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.