cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F411C minimal wiring?

BSchm.6
Associate III

Hi,

I'm currently moving a project from STM32F446 to an STM32F411CEU and stumble upon some strange things in the wiring which is not known from the F446.

So from the manual it is not clear to me how to deal with the VCAP_1 and PA0-WKUP inputs.

So my question: is there some documentation/schematic available that shows the minimal wiring of the 48-pin F411? I know there are some eval-boards out there but their schematics are far away from being "minimal".

Thanks!

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions

Hi @BSchm.6​ ,

Looking for documentation, you need to refer to AN4488: Getting started with STM32F4xxxx MCU hardware development.

-Amel

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

3 REPLIES 3

Basically supplies, ALL

VCAP single pin 4u7 or 2u2 on each. Expect to see 1.25V on them when working.​

​

P​ull BOOT0 LOW

​

And then whatever programming interface you use.

Tips, Buy me a coffee, or three.. PayPal Venmo
Up vote any posts that you find helpful, it shows what's working..
BSchm.6
Associate III

OK. And how about VREF+ (when no VREF- is available?) Connect with 3.3V?

Hi @BSchm.6​ ,

Looking for documentation, you need to refer to AN4488: Getting started with STM32F4xxxx MCU hardware development.

-Amel

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.