Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
HiI have a problem with my board with STM32L496ZGT6.Some boards works fine (so.. i think there isn't a project problem) some boards are in loop during the power on.I exaplin better:Here a function in main.cpp: /*Configure the main internal regulator...
Hallo,until now we have used STLINK-V3SET connected with MIPI10 to custom evaluation board based on STM32H743.For next custom board we need cost efficient debugger solution, just like STLINK-V3MODSBut it seems not to work together.MIPI10 connector us...
Hello,I have finally received a voucher to get a free NUCLEO-H563ZI board when attended workshop "STM32H5: Ultimate combination of performance, integration and affordability".Despite following the procedure provided in mail I'm unable to get past Pla...
Hi,We are now using NXP mcus for our smart lighting products, and decide to use STM32 mcus for instead from now, I bought one Nucleo-STM32G070, one Nucleo-STM32F103, and one Nucleo-STM32F767. The most challenging work for us is to build a TCP/IP appl...
Hello everyone, I hope you're all doing well. Recently I have tried to measure temperature using a K-type thermocouple with a breakout board that uses a MAX31855 IC Its sends out 32 bits and my board can read 32 bits SPI. I have wired everything corr...
Hello FreeRTOS friends,I'm back seeking guidance. I want to mention that I've configured this project without using the IDE, by manually setting up the necessary ETH pins for its operation.I've followed the documentation on the page, but I'm unable...
Before ST started bricking counterfeit st link V2 units, I was able to program my board without issue. I bought a confirmed genuine ST Link V2 from RS components and connected it exactly as shown, but it never connects to the target and all I can get...
Hi,I just bought a Necleo-STM32F767ZI board, and downloaded the example "LwIP_HTTP_Server_Netconn_RTOS" in CubeIDE, and made following changes in main.h:#define IP_ADDR2 3#define GW_ADDR2 3As for the board, I did not make any changes on the jumpers...
Hello !I looking for a cellular shield for my project that would fit on my Nucleo-L152RE board. Does the ST company produce something similar and is it possible to buy it ? Sincerely,Maxim
HiI'm following the UM2692 to start a develop with the STSPIN32F060x.I just have the STEVAL-CTM011V1A board and the STLINKV3 with the isolator adapter and a 1/6HP three phase motor.I started the "Fimware Debug" part on the UM2692, page 7.Perform the ...