Resolved! NUCLEO-C5A3ZG STM32C5 QSPI Display Bring up Project
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.
This project tests the STM32C5's XSPI capability to drive QSPI display using the NUCLEO-C5A3ZG M.2/SerialMem connector. GitHub - stm32-hotspot/STM32C5-M2-Serial-Mem-QSPI-Display · GitHub
Hello, hope everyone is well. I'm working on the software side for a micro mouse bot. We're planning on using the STM32G070RB for the microcontroller. For prototyping, I'm using the NUCLEO-G070RB. I separated the ST Link from the board, and wired t...
Hey team,I am working on a project using the STM32F103CB MCU. The device operates from both USB and battery power. The battery configuration consists of four 1.5 V alkaline cells arranged as 2S2P, providing a nominal 3 V supply. USB power is provided...
Hello STM Community,I'm facing an issue with my STM32 device on Windows 11. The Virtual COM Port (VCP) driver is not working, and in the Device Manager, the device is shown as:Unknown USB Device (Device Descriptor Request Failed)Here are the details:...
Im using i2c on stm32 nucleo and the slave is a cheap imu (mpu6500). Sometimes the bus just gets stuck and doesnt work. And the weird thing is if i plug everything out, flash code again and run it it will not work. Until it randomly works again until...
Is there a board schematic for STM32L432KC somewhere?I want to acces pin PA13. But I can find no connector or easy acces point.Thanks
i am quite new for stm32n6, i am working with STM32N6570-DK with Arduino IMX335 . i just wanna make a simple snaphort using the project SnapshotDecimationMode (used with mb1854)as my reference. i can configured the camera via I2C and start the pipe. ...
While designing Electronic speed controllers for a 6s battery, an stm32 was decided to use as the MCU. After receiving our first PCBs, we were unable to successfully program them with the stlinkv3 minie. Attached is an image of the schematic of wh...
hi, ive noticed that hand landmarks pre built binarys uvc output does not work on the C02 revision NUCLEO-N657X0-Q but does work on the c01 rev, could anyone guide me on how to get this demo up and running ont he c02?
Dear all, I would like to connect a camera to my Nucleo F756ZG board, with the goal to send images via the ethernet port. However, this board doesn't feature a 30-pin ZIF connector nor a 22‑pin FFC connector....Apparently, the STM32 F756ZG has a "DCM...
So as the title suggests, I have been trying to get the LCD screen to work on the STM32F469i-DISCO board. Currently I just want it to turn on at all. I found the BSP drivers in this link as well as the OTM8009A drivers in this other link When I run ...