STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Using RC522 module on STM32F401

Hello,For a school project, I am trying to use the module RC522 module to do RFID tagging with a Nucleo F401RE. I had some issues to do it and was wondering if anyone has a good library with this board.If needed, I can provide you my code.

Hippo by Associate
  • 4673 Views
  • 3 replies
  • 0 kudos

Designing custom Board

Hello,for a DIY project including LoRa ra-02, MPU6050 and NEO-6M i have purchased some Blue pills from a vendor but it turned out they are fake blue pills (STM32F103C6).I am trying to make a RC, so i have a Transmitter which needs 2xSPIs (one for LoR...

hamo by Senior
  • 2957 Views
  • 8 replies
  • 1 kudos

Resolved! STM32H7B3I-DK CubeMX Board Configuration

In using CubeMx 6.11.0 to start a new project for the STM32H7B3I-DK to use the USB OTG, I noticed that none of the USB_OTG_HS_ULPI_xxxx pins are configured. The USB_OTG_HS peripheral option is not allowed because of an I2S6 conflict. Now I'm wonderin...

maynarde by Associate
  • 1914 Views
  • 3 replies
  • 0 kudos

Resolved! stm32H745i-disco board lwip + freertos + stmcubemx 6.10 code generation guide

i wand to work on ethernet of stm32H745i disco board , i need to generate code  lwip + freertos using toolstm32cubemx version 6.10.0 please give simple demo working project that generated by stm32cubemx version 6.10.0or guide me how to enable lwip an...

USB CDC Increase Reading Speed

Hello,I'm currently working on a USB project and i encounter some issues. I would like to send data to the STM32 and the STM32 must re-send it as fast as possible. I already test the sending speed and it work great for me but the reading speed is low...

Kakyouka by Associate II
  • 5076 Views
  • 9 replies
  • 0 kudos

SD card not detect in fp-ai-vision1

I am using STM32H747-DISCO with the FP-AI-VISION1 package, I have updated my drivers and solved the screen problem. Now I am facing an issue with the SD card. It is given that an SD card with class 10 is recommended, I am using SanDisk Ultra microSDH...

IMG_20240314_160717427~2.jpg IMG_20240314_160842963~2.jpg