Hi,My application used ST25R3916B for transmit power for the card only.1. Is it possible to leave the EXT_LM pin unused or exclude external load modulation from my application?2. Can I use the testing point only on the pin EXT_LM pin?Best,Dalik LIM
Hi, In AN4974 (antenna matching network for ST29R391x device), In chapter 6.2.1 in Simulation S-parameter and Transition model, what is the tool used for simulation in this case?Best,Dalik
Hi, My application used ST25R3916B for transmit power for the card only.1. Is it possible to leave the EXT_LM pin unused or exclude external load modulation from my application?2. Can I use the testing point only on the pin EXT_LM pin?Best,Dalik LIM
Hi,My Application of STM32G0 is used for developing the product NFC reader.1. Can you recommend the reference hardware design for STM32G0B1CCT6?best,Dalik LIM
Hi, In AN4974 (antenna matching network for ST29R391x device), In chapter 6.2.1 in Simulation S-parameter and Transition model, what is the tool used for simulation in this case? Best,Dalik