cancel
Showing results for 
Search instead for 
Did you mean: 

Internal and External Clock of STM32G0

Dalik
Associate III

Hi,

1. Why some configurations of STM32G0B1CCT6 don't use an external clock for HSE?

2. STM32G0b1 can support USB C PD protocol?

best, 

Dalik LIM

This discussion is locked. Please start a new topic to ask your question.
3 REPLIES 3
Peter BENSCH
ST Employee
  1. Can you please give some information on which configuration you think does not support HSE?
  2. Yes, G0B1 supports UCPD.

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

1. STM32G0 Discovery kit for USB Type-C™ and Power Delivery in UM2401.

Best, 

Dalik LIM

Peter BENSCH
ST Employee

Well, the STM32G071B-DISCO gets its clock from the MCO of the included ST-LINK/V2-1 via SB5. If you actually really want to rebuild the DISCO and use the HSE, you have to remove SB5 and populate components X3, R41, R44, C42 and C43.

Hope that helps?

Good luck!
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.