STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32F469-DISCO revision confusion

HiI own a STM32F469-Discovery Board bought in 2021. There seem to be (at least) two revisions of that board, "B" & "C" and maybe "A". Under "CAD Resources" are just schematics for Revision "B" and "C".If I try to run the supplied example for that boa...

PGroe.2 by Associate III
  • 3492 Views
  • 6 replies
  • 0 kudos

GPIO Pin not going High

I'm using a Nucleo-H723VG board and trying to use the PB8 and PB9 pins. I'm able to set PB9 high and see a voltage of 3V but for PB8 it only shows a voltage of 359mv. I have tried enabling the internal pullup and still doesn't go high to 3V.The yello...

jasd33p_0-1725464875313.png
jasd33p by Associate II
  • 3547 Views
  • 9 replies
  • 4 kudos