STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! 4-bit SD card communication STM32H723

Hi all,I am designing a PCB around the STM32H723 and wants to implement 4 bit SD card communication. As shown in the picture it can be done using 3.3V, with lower speeds, and avoiding these fine-pitch level translators. However does anybody have expe...

elso_0-1714991791468.png elso_0-1714992932946.png
elso by Senior
  • 1641 Views
  • 1 replies
  • 0 kudos

Resolved! STM32F723VET6 Find a circuit diagram

Hello.Looking for a reference circuit diagram of STM32F723VET6.If not, I'm looking for a circuit diagram of 32F723 EDISCOVERY.Please give me a link.The reason is that I want to use vdd as 1.8V instead of 3.3V, but I want to refer to it. think you.

leenaya by Associate
  • 2989 Views
  • 6 replies
  • 7 kudos