STM32 MCUs Boards and hardware tools

Ask questions and find answers on STM32 hardware set-ups, including schematic-related challenges, debugging probes, power configurations, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ST-LINK V3 firmware and licensing

We are designing a board for internal product development and testing (not for sale) based on NUCLEO-U575ZI-Q (the Altium source). We aim to manufacture a handful of boards for internal use during development. We will re-use parts of the existing des...

MikeStrom by Associate II
  • 1726 Views
  • 2 replies
  • 3 kudos

Resolved! STWINBX1 loses RTC at poweroff?

HiI have found that the STWINBX1 loses RTC at poweroff (or does CubeMX write code to reset RTC at poweron? there is a ticket on that) so that I have to battery-power it on, connect usb, update RTC and then disconnect while still on in order to log wi...

STM32F446RE CRC mismatch

Hi, I am following a video to write a bootloader that transfers the application code serially into the STM32F446 controller. The video originally presents the STM32F7xx series controller, but I am applying it to the F4xxx series. I have modified the ...

FShah.1 by Associate III
  • 4796 Views
  • 10 replies
  • 1 kudos

Resolved! NUCLEO-H753ZI voltage output

Hello, Can I output an adjustable voltage ranging from -10V to 10V using the h753zi development board? I found something like a "PWM to 0-5V/10V DAC Module."Would I need to use such an external module or build an additional circuit externally to achi...

HMsDobby2 by Associate III
  • 1605 Views
  • 1 replies
  • 1 kudos

Programming NUCLEO-F303ZE with JTAG

Hello, I made a code to readout all the STM32 ADCs. The code works.I want to run it on my Nucleo-F303ZE with JTAG ProVision, but it dont work.What did I do wrong?I connected it like this:JTAG               NUCLEOTCK     =>        SWCLK-JTCK (PA14)TMS...

SFentro_X_1-1732893823786.png SFentro_X_2-1732893964023.png

STM32f446re Altium

Hello everyone, I’m currently working on a project involving the STM32F446RE as the main microcontroller. It’s my first time using Altium Designer, and I’ve been searching for the footprints and schematic symbols for the components I need. While I’ve...

Soniaa12 by Associate
  • 2715 Views
  • 1 replies
  • 0 kudos