2020-11-19 12:41 AM
I'm using the dfu bootloader, but I can't figure out the cause.
I entered the address value of the bootloader as well as the address value (0x08010000) of the application and the offset after viewing several posts.
It works if you proceed with the following procedure.
-1- Download the applicaion (custom software) with st-link.
-2- Erase the all memory.
-3- Download the bootloader application with st-link.
-4- Upgrade the created dfu file with the dfuse program.
If you proceed with the above procedure, the execution goes well.
However, if you add an image to the application and recreat the dfu file and
step -4- is executed, it will not run.
Do you have any predictions about the problem?
p.s : UI work was done using touchgfx and cpu model is stm32f746g-discovery.
2021-01-16 2:17 AM
Have you solved this problem?