cancel
Showing results for 
Search instead for 
Did you mean: 

Custom bootloader. MCU STM32H7BIT Application use FreeRTOS and TouchGfx. Some issues.

ANapa
Associate III

Hi,

I build a custom bootloader.

Trying to load app on FreeRTOS and TouchGfx

MCU - STM32H7BIT

The MCU has 2 FLASH banks:

0x08000000 - 1024k

0x08100000 - 1024k

gcc-arm-none-eabi toolchain.

openocd for loading and debuging.

The app works fine when loaded at 0x08000000. FLASH origin.

Next...

Begin Option 1:

-------------------------------------------------- --------------------------------------------------

The application works after loading from the bootloader if stored at 0x08100000.

I do in bootloader:

void Bootloader_JumpToApplication (void)

{

     HAL_RCC_DeInit();

     HAL_DeInit();

     /* Disable SysTick */

     SysTick->CTRL = 0;

     SysTick->LOAD = 0;

     SysTick->VAL = 0;

     __asm("B 0x0812E700"); // Address obtained from *.map file

                // This is the address of Reset_Handler

}

In the application *.ld file

FLASH(rx): ORIGIN=0x08100000, LENGTH=2048K

SCB->VTOR = 0x08100000; By some miracle. Without my participation.

However I do:

SCB->VTOR = 0x08100000; At the very beginning of main(), in the application, just in case.

-------------------------------------------------- --------------------------------------------------

End Option 1:

Begin Option 2:

-------------------------------------------------- --------------------------------------------------

Does not work!

Application downloaded at 0x08060000

In the application *.ld file

FLASH(rx): ORIGIN=0x08060000, LENGTH=2048K

In the bootloader:

void Bootloader_JumpToApplication (void)

{

     HAL_RCC_DeInit();

     HAL_DeInit();

     /* Disable SysTick */

     SysTick->CTRL = 0;

     SysTick->LOAD = 0;

     SysTick->VAL = 0;

     __asm("B 0x0808E890"); // Address obtained from *.map file

                 // This is the address of Reset_Handler

}

SCB->VTOR = 0x08060000; At the very beginning of main(), in the application.

QtCreator memory viewer shows that this measurement value in the SCB->VTOR area is correct.

Application continues to run...

After that, a Hard Fault occurs.

Undefined instruction (UNDEFINSTR)

Invalid function call address 0x58024400 - Very strange address!

XPSR 0x41000003

PC 0x80014FA - Very strange address!

SP 0x2001FFBC

-------------------------------------------------- ----------------------------------

End Option 2:

Begin Option 3:

-------------------------------------------------------------------------------------

If exclude the TouchGfx task from the application, then everything works with any place of the applications.

At the same time, FreeRTOS works:

osThreadDef(touchTask, taskTouch, osPriorityNormal, 0, 128);

touchTaskHandle = osThreadCreate(osThread(touchTask), NULL); // Tracks i2c touchscreen events

osThreadDef(logTask, taskLog, osPriorityNormal, 0, 128);   // Send debug strings to UART6

logTaskHandle = osThreadCreate(osThread(logTask), NULL);

I can rewrite all SDRAM by touching the touchscreen.

Screen fill colors change as I conceived and programmed.

UART6 prints my debug lines

-------------------------------------------------------------------------------------

End Option 3:

The problem is in TouchGfx???

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
ANapa
Associate III

It seems that the problem was solved by careful selection of smaller stack sizes for FreeRTOS tasks.

Downloads of various applications with a custom loader now work.

View solution in original post

1 REPLY 1
ANapa
Associate III

It seems that the problem was solved by careful selection of smaller stack sizes for FreeRTOS tasks.

Downloads of various applications with a custom loader now work.