wrong capacity
After upgrade ST-Link firmware to 2.37.26, the drive capacity did not display correctly. On the screen - to boards Nucleo-64 F446RE and G474RE
After upgrade ST-Link firmware to 2.37.26, the drive capacity did not display correctly. On the screen - to boards Nucleo-64 F446RE and G474RE
Hi, I tried to upgrade the firmware for my ST-LINK 3 SET (using the STLinkUpgrade came with STM32CubeProgrammer) and something went wrong (didn't do anything special, just clicked "Open in update mode" and then "Upgrade"). Now its "Version" appears t...
Getting a "Error: Bridge error (BRG_CAN_ERR)". Can't find any documentation about it.The StmLinkV3 is able to program the Nucleo (Stm32H743) via SWD fine. In the screenshot's log section, the first message shows that the StLink doesn't detect the...
Nucleo-H743ZI2 Dev BoardSTM32CubePRogreammer V2.3, and V2.4OS: Windows 10 Using CubeIDE with a new board I get the popup saying that the board needs an update. The IDE was unable to successfully do this. So I attempted CubeProgrammer 2.3 with no luck...
Hi, I have 2 Nucleo boards: NUCLEO STM32F767ZI (F4) and NUCLEO STM32F446RE (F7).I'm using macOS 10.15.4 omn MacBook Pro 2017 with STM32CubeProgrammer 2.4.0 and stlink tools from brew (GitHub.com/texane/stlib).When I plug in F4 over USB-C to USB-Mini ...
HelloI implemented an external flashloader for STM32F767 for an external SPI Flash. The size of the flash is 256MBit. I want to readout the whole flash with *.bat file. I tried with this line:STM32_Programmer_CLI.exe -c port=SWD reset=HWrst freq=800...
Hello,I want to program (first time) an STM32F042K6 with STLINK-V3SET using SWD.When I try to "connect" with STM32CubeProgrammer, I get these informations : "Error : No STM32 target found!". Here is a screen :The connections are : I tried to run the ...
The St_link registers itself and the serial is updated etc. however when I attempt to connect to the newly soldered chip, I get the message that "No STM32 target found".Am I attempting to program this chip incorrectly by using the SWDIO, GND, SWCLK a...
So I just recently got an stm32f103c8t6, and I was able to connect to it with the serial pins connected to pins A8 and A9, but for whatever reason, I was not able to get it to connect with the St link v2 that I also ordered. For connections, I connec...
Hello All,I am using "STM32F746G-DISCO" Kit and i would like to program the GRAPHICS DATA on external flash.i compile my firmware in Release Mode, I need to load program externally using STLink Or STM32Cube Programmer.I need to program external flash...