STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

STemWin drawing artifacts

Posted on May 23, 2014 at 00:29Hi, I just spent a couple of days integrating STemWin in a starter project and got that to work rather nicely. Now I am toying around with it so see if it can do all the things I need for my display project. In the pro...

elmar by Associate II
  • 2477 Views
  • 5 replies
  • 0 kudos

STM32F429I-DISCO LCD and DCMI

Posted on December 01, 2013 at 11:20Hi All!I just bought an STM32F429I-DISCO eval board because of the LCD screen, and wanted to use it with a Camera on the DCMI interface. I found out that there is conflict in the pin-out, e.g. LCD_VSYNC and DCMI_H...

jeno by Associate II
  • 2845 Views
  • 6 replies
  • 0 kudos

How could I use a keyboard with STemWin?

Posted on May 23, 2014 at 11:59What should I do first?2 Tasks: one sends key msg, one keeps running GUI_Delay().But, The Callback just keep silent with user defined key ID.Am I miss something?Of course, I know make it OnFocus first. #stemwin

Microstar by Associate III
  • 904 Views
  • 1 replies
  • 0 kudos

Help CubeMX HAL and DMA2D

Posted on April 03, 2014 at 14:41Hi. Help is needed for Alpha channel input (CM_A4 an CM_A8) in combination with the HAL_DMA2D_BlendingStart(...) of the CubeMX HAL. It seems like FGCOLR is not set neither with the call nor with Dma2dHandle.LayerCfg....

arm by Associate
  • 1687 Views
  • 3 replies
  • 0 kudos

STM32F429 EvoPrimer Design Contest

Posted on November 01, 2013 at 18:34To  any STM32 users who might be interested, The 2014 Application Design Contest for the STM32F429 EvoPrimer started 31 October. You can win from $10 000 in cash prizes for your application!STM32F429 applications ...

STM32F205 DCMI

Posted on May 15, 2014 at 13:27Hello Forum, I do have a STM32F205VE device 100Pin Package to which i connected a Camera as to the DCMI Interface. From the DCMI Status register i can tell, that HSYNC and VSYNC are detected. However, nothing is captur...

STemWin Window updates

Posted on May 12, 2014 at 22:12I'm implementing the touch screen calibration screens that are found in the demo project in my project on the STM32F439-EVAL platform. I'm having some trouble drawing screens in the window manager callback and I'm not ...

kartik by Associate II
  • 1105 Views
  • 1 replies
  • 0 kudos

stemwin double buffering glitch

Posted on April 28, 2014 at 18:49Hi there, i'm trying to use stemwin with double buffering on a STM32F429. Unfortunately there seem to be glitches when drawing. Stemwin is configured with the correct frame buffer address and the mechanism of switchi...

philipp by Associate II
  • 1165 Views
  • 1 replies
  • 0 kudos

UNABLE TO DISPLAY IMAGE ON 240x320 TFT DISPALY

Posted on May 05, 2014 at 06:22Can some one help me out  as I am unable to display image on HY32D TFT.The TFT Display controller is ILI9320 and ''LCDVision'' is used to convert image into c array.Is there any turn around to this problem ?Hardware an...

soobia by Associate II
  • 2815 Views
  • 7 replies
  • 0 kudos