STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Unable to link emWin - missing LCD_IO_WriteReg

Posted on April 07, 2016 at 13:15I'm trying to build a first graphical LCD project with Visual GDB (which lets you use Visual Studio for embedded development using the ARM GCC toolchain). I can't find any sign of any of the LCD_IO_ routines in the ...

LCD Refresh Rate

Posted on April 11, 2016 at 12:51Hi, I'm using a Discovery board with an STM32F469NI on it. I'd like to know more about how to set the LCD display refresh rate to a particular value. I've been through the spec sheet and reference manual and there's ...

aditya23 by Associate II
  • 2178 Views
  • 4 replies
  • 0 kudos

JPEG Display Error

Posted on April 06, 2016 at 08:35Hello, When I try to draw JPEG�s I get a faulty display.http://www.ecs-online.dyndns.org/Uploads/Original.jpghttp://www.ecs-online.dyndns.org/Uploads/Incorrect.JPG MS_LoadFileIntoMemory(&fileNames[currentSel][0], arr...

fjahn9 by Associate II
  • 851 Views
  • 0 replies
  • 0 kudos

emWin HardFault Issue

Posted on April 04, 2016 at 20:10Hello,I have made custom board with stm32f429 without external SDRAM.I'm trying to drive 4.3'' TM043NDH02 16.7M color TFT. In my first try I have took as an example of emWin ''Hello World'' demonstration under stm32f...

DSI using Standard Periph Library

Posted on March 27, 2016 at 04:22I've recently started working with the STM32F469 Discovery board with the intention of checking out using DSI to drive an LCD. The examples I've seen for DSI are all HAL-based and I was wondering if there was any doc...

About the STemWin of the STM32F4 Discovery.

Posted on March 26, 2016 at 18:09I used the STemWin_SampleDemo from the STM32F4 Discovery SDK to run my program. I find out that if I put WM into menu controls, when I delete(WM_DeleteWindow) the menu widget, that MCU will appear HardFault_Handler. ...

yaomei65 by Associate
  • 761 Views
  • 0 replies
  • 0 kudos

Is this a bug in the HAL DCMI driver?

Posted on March 07, 2016 at 16:52 This is from the 1.0 driver. (I'm downloading the next version but it is going. Real. Slow.) From STM32Cube\Repository\STM32Cube_FW_F4_V1.0\Drivers\STM32F4xx_HAL_Driver\Src\stm32f4xx_hal_dcmi.c ...

hbarta2 by Associate III
  • 1012 Views
  • 2 replies
  • 0 kudos

stm32f103 and winstar TFT display problem

Posted on March 09, 2016 at 14:24Hi all, I have problem with displaying any data at WF57STIACDNN0 TFT display. This is a TFT display with ST7511U driver. In my SW driver I successfully pass the display initialization procedure - I see some randomize...