Skip to main content
bazookafighter
Associate
March 11, 2016
Question

[Bug] STM32F469I-Discovery BSP: LCD Orientation

  • March 11, 2016
  • 1 reply
  • 869 views
Posted on March 11, 2016 at 10:36

By default, if one uses the

BSP_LCD_Init()

function provided by the library ''stm32469i_discovery_lcd.h'' to set up the LCD screen of an STM32469I-Discovery board, the screen orientation will be landscape. If one wants to change it to portrait instead, he or she will have to use

BSP_LCD_InitEx(LCD_ORIENTATION_PORTRAIT)

but unfortunately that does not work and all you will get is a blank screen because there is a bug in said function. As it turns out, some settings within the function were mixed up. The following is the corrected version which fixes everything and finally gives users the ability to switch to a portrait orientation. The problem can be found beginning from line 252 of the source code ''stm32469i_discovery_lcd.c''.

/* Timing parameters for all Video modes
* Set Timing parameters of LTDC depending on its chosen orientation
*/
if(orientation == LCD_ORIENTATION_PORTRAIT)
{
VSA = OTM8009A_480X800_HSYNC; //Originally OTM8009A_480X800_VSYNC;
VBP = OTM8009A_480X800_HBP; //Originally OTM8009A_480X800_VBP;
VFP = OTM8009A_480X800_HFP; //Originally OTM8009A_480X800_VFP;
HSA = OTM8009A_480X800_VSYNC; //Originally OTM8009A_480X800_HSYNC;
HBP = OTM8009A_480X800_VBP; //Originally OTM8009A_480X800_HBP;
HFP = OTM8009A_480X800_VFP; //Originally OTM8009A_480X800_HFP;
lcd_x_size = OTM8009A_480X800_WIDTH; /* 480 */
lcd_y_size = OTM8009A_480X800_HEIGHT; /* 800 */ 
}
else
{
/* lcd_orientation == LCD_ORIENTATION_LANDSCAPE */
VSA = OTM8009A_800X480_VSYNC; /* 12 */
VBP = OTM8009A_800X480_VBP; /* 12 */
VFP = OTM8009A_800X480_VFP; /* 12 */
HSA = OTM8009A_800X480_HSYNC; /* 120 */
HBP = OTM8009A_800X480_HBP; /* 120 */
HFP = OTM8009A_800X480_HFP; /* 120 */
lcd_x_size = OTM8009A_800X480_WIDTH; /* 800 */
lcd_y_size = OTM8009A_800X480_HEIGHT; /* 480 */ 
}

P.S. Tested with STM32CubeF4 v.1.0 #discovery #tft #stm32 #lcd
This topic has been closed for replies.

1 reply

Amel NASRI
ST Technical Moderator
March 29, 2016
Posted on March 29, 2016 at 16:34

Hi tfl,

Thanks for bringing this issue to our attention and also for the suggested solution.

This is already reported internally.

-Mayla-

To give better visibility on the answered topics, please click on "Best Answer" on the reply which solved your issue or answered your question.