STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

STemWin - GUI_JPEG_DrawEx

Posted on January 24, 2017 at 13:17Hi.I'm using STM32CubeF4 1.14.0 with STemWin 5.32.I need to draw JPEGs from file using the DrawEx functions where the user has to provide a getData function which reads chunks of data from a file.However the ...Dra...

bbee by Associate III
  • 5401 Views
  • 11 replies
  • 0 kudos

Resolved! STM32CubeMX FSMC Configuration

Posted on March 15, 2017 at 02:13I'm using a Nucleo-F413ZH board and an SSD1289 driver based LCD. I'm using the KEIL IDE.I just wanted to confirm that I have setup my LCD and FSMC correctly. I have performed the following steps: Setup FSMC in STM32...

STM32F407, DMA2 IRQ versus TIM3 IRQ, TIM3 wins!

Posted on March 09, 2017 at 13:34Hi to all,I am developing a graphic driver that handle 2 LCD over the SPI1 port and different CS lines. I setup a frame renderer tat renders 128 scanlines made of 160 pixels. A frame rendering can be launched by the ...

Digimorf by Associate III
  • 2811 Views
  • 6 replies
  • 0 kudos

STM32 DMA Limitation ?

Posted on March 08, 2017 at 06:34Application Scenario: We have used DMA, FSMC, and DCMI module of the  STM32. DMA is configuredto read the data from the DCMI out output  register DR, and write it it to external SRAM. Likely DCMI is configured  as an...

Connect STM32 FSMC to LCM with 6800 interface

Posted on February 24, 2017 at 12:04I want to use STM32 to drive a LCM with a KS0108 controller. Sadly, it has a 6800 interface. Fortunately, ST gives a document to guide me: http://www.st.com/content/ccc/resource/technical/document/application_note...

0690X00000606P6QAI.png 0690X00000606PLQAY.png

STM32F407, DCMI_DMA,USART_DMA

Posted on February 24, 2017 at 08:19I am transferring 240x320 image in RGB565 format to USART.But unable to get full image because USART speed is not matching with DCMIPixel Clock for DCMI_DMA:12MHzUSART speed:921600I am using DCM_DMA in snapshot,ci...

Nagesh K by Associate II
  • 1388 Views
  • 1 replies
  • 0 kudos

STM3221G-EVAL and SSD1963

Posted on December 11, 2014 at 17:08Hi:I am using the STM3221G-EVAL board and trying to use a a different TFT display than the original that came with the board. The original display is an Ampire display that uses a Ilitek controller ILI9320.The new...

eduardo2 by Associate II
  • 2063 Views
  • 3 replies
  • 0 kudos

Resolved! How to toggle the Ax pin when using fsmc

Posted on February 20, 2017 at 00:30I am trying to implement FSMC in order to drive an ili9341 LCD in 8080 mode. However to distinguish between command and data I need to toggle the RS(register select pin) which according to reference manual AN2790 ...