STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

STemWin Execute Button

Hello,I have been experiencing the following issue when working with CubeMX :#1. The EXECUTE button of the Graphics Middleware / STemWin Configuration panel does NOT open the GUI Builder, when it is clicked (activated). GUI Tool is enabled.Here is th...

Sue.Jay by Associate II
  • 2899 Views
  • 8 replies
  • 0 kudos

Resolved! Multiple displays possible?

Is it possible to create any kind of hack to run multiple displays on one MCU with ToughGFX?I'm looking for a way to have one display be drawn normally, but with two smaller displays at very low frame-rates (no higher than 1Hz).

Using external hardware buttons

I am wondering if there are any examples or plans to add functionality to the external buttons in TouchGFX Desiger.In the beginning of last week I succeeded in touch control by applying my GUI to the 746dico board. And now I am connecting the externa...

YJMoon by Associate III
  • 2342 Views
  • 6 replies
  • 0 kudos

STM32L4R9I-DISCO with new ST7796H2 display driver

Working on getting a new TFT DSI LCD display to work on the STM32L4R9I-DISCOVERY kit. It uses the ST7796H2 display driver. emWin shows they have added support for this in their 5.36 version in the GUIDRV_FlexColor files, but STemWin is only reved to ...

Du1 by Senior
  • 7500 Views
  • 17 replies
  • 0 kudos