STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

DMA2D with 8-bit output pixel format

I'm trying to hook STM32F767 (on a Nucleo-144 board) to a 640x400 24-bit LCD-TFT display with the following configuration:use the controller's internal RAM to store framebuffer, and drive the display using the LTDC controlleruse 8-bit pixel format wi...

MGode by Associate
  • 1604 Views
  • 1 replies
  • 0 kudos

Support for a keyboard widget

Hi,I wanted to know if you've any future plans of creating a keyboard widget? It'd drastically simplify the devolpment process of GUI interfaces for touch screens as creating a fully functional keyboard with all the functionalities one would expect o...

GMeur by Senior II
  • 2422 Views
  • 6 replies
  • 0 kudos

Support for STM32H743I-EVAL

Hello,I'm using the STM32H743I-EVAL. I want to use TouchGFX in my program, but I can't find any project template to start from. If there were some basic "Hello World" program, that runs out of the box on the evaluation board, that would make my life ...

SSagi by Associate II
  • 2984 Views
  • 6 replies
  • 0 kudos

[Feature Request] Implement Background Widget so the Slide transition only slides the other widgets but not the background.

Pretty advanced feature I'm requesting here, but would it be possible to have a Background Widget so it can be excluded from the Slide screen transitions? This way, if we have an application with multiple screens that all have the same background ima...

Plaramee by Associate III
  • 1423 Views
  • 3 replies
  • 1 kudos

Canvas buffer

Hello,I have such kind o problem with my application which contains of many screen. One of these screens is quite complicated (many modal windows, buttons, list, etc). When I call xQueueSend to forward messages between two tasks (one relates to uart ...

Marcin1 by Associate II
  • 1861 Views
  • 4 replies
  • 0 kudos

Having trouble with DMA2D and TFT LCD

I have a project running an STM32F429, and I have a TFT LCD connected using the FMC subsystem. (I'm not using the LTDC because I'm using that for another LCD). This LCD is an 8080-type interface with 16-bit wide data, /RD, /WR, /CS and command/data s...

STM32L4R9I-DISCO SD storage not working

I have a TouchGFX project created from TouchGFX for the STM32L4R9I-DISCOVERY and I'm editing the code to enable storage for playing audio. However, when I enable Storage_Init(MSD_DISK_UNIT); either from main.c or using the mmi_interpreter with: MMI_I...

Du1 by Senior
  • 983 Views
  • 2 replies
  • 0 kudos

Resolved! ST32L4R9I-DISCO Demo Code

Hello,I would like to use a lot from the ST32L4R9I-DISCO Demo Code for my own application.Are you planning to release the source code?Thanks and best regards,Christoph