STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

View class inheritance

Hello,I am working now on project where screens have many things in common (slide menus, content etc). Is it possible to make a screen which will be the base class for further screens? Or I should make it a custom container?

maciek by Associate II
  • 1577 Views
  • 2 replies
  • 0 kudos

STM32F769I-Disco with CubeMX + sw4stm32

Hello,I have tried to generate a simple GUI with touchgfx, CubeMX and sw4stm32 for stm32f769I-Disco. I used the guide "Configuring STM32F769I-Disco" from TouchGFX I have also read the Tutorial 10 from UM1718. But the GUI on the Screen does not look l...

0690X0000087qesQAA.png 0690X0000087qdQQAQ.jpg

DSI custom board problem with STM32F769BI MCU

Hello,I used STM32F769I-EVAL board as a design reference for custom board. However, I could not achieve correct operation of MB1166 LCD board which is connected via DSI. It works well on the evaluation board.When MCU tryies to display a picture, scre...

GSink by Associate II
  • 18557 Views
  • 16 replies
  • 0 kudos

Interfacing custom touch controller... Advice needed

Hi colleagues,I'm facing some problems interfacing the I2C touch controller of my LCD dislay.The board's LCD works perfect using only MXCube for hardware configuration and Attolic to debug.Please give me advice what will be the best way to make a cu...

HBosh by Associate
  • 1101 Views
  • 1 replies
  • 0 kudos

moving to different package STM32F429ZI -> STM32F429II, is there anything to change on TouchGFX BSP?

hi, i'm developing a TouchGFX Designer based app on STM32F429I-DISC1 that's based on STM32F429ZI LQFP144 pin MCU. so far so good, but..we need more IO pins to they told me our custom board will be based on STM32F429II which is LQFP176. i asked them t...

Resolved! Keil folder doesnt exist

Hi guys, I have a STM32L4R9I-DISCO board. I create a touchgfx project from Application Template for this disco board. After that I can run simulator, generate code and run target without problem. I can see my application in disco board's LCD. I wi...

Epamuk by Associate III
  • 1515 Views
  • 1 replies
  • 0 kudos

STM32CubeMX 5.1.0 generate incorrect code for LCD

Hi,there is a bug of CubeMX I Found:I’m using STM32CubeMX5.1.0,and STM32CUBE_FW_L0_V1.11.0when creating a project for stm32l073, In ‘LCD Mode and Configuration’ dialog, ‘Multiplex Mode’ checkbox takes no effect. Whether it is checked or not, CubeMX ...

CGuo by Associate
  • 1452 Views
  • 1 replies
  • 0 kudos