STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

STM32L073 HAL_LCD_Write function

Posted on November 29, 2017 at 09:01Hello,I'm working on a custom board : stm32l073 + LCD screen ( matrix 4 x 25 ).I can't understand how to use HAL_LCD_Write function.As far as I understand I just need 3 parameters in order to write LCD : COM: 0-3 ...

moranf by Associate II
  • 4206 Views
  • 5 replies
  • 0 kudos

Build FreeRTOS error

Hi everyone,I'm using STM32cubeMX + TouchGFX on the STMF746-DISCO.And with a basic project generate by the STM32cubeMX, I have this error :"Error: expected '=', ',', ';', 'asm' ....Without FreeRTOS in a project, the error disappear !I suppose there's...

0693W000000Tu9qQAC.png
LSylv by Associate II
  • 891 Views
  • 1 replies
  • 0 kudos

Problem with downloads to STM32F746G DISCO and TouchGFX demonstration program from FW F7 V1.16.0 repository

Hello, demo project is prepared for SW4ST32. After importing I can build all files without any problem.Then trying download (by Debug option from menu) I have achived some problems - but it seems that is flasded. On DISCO there is nothing until reset...

Set widget visible doesn't work properly

Hi,I have a problem when I want to make a widget visible.This code works :myStructure test; widget.setVisible(test.state); // test.state = bool widget.invalidate();But this code doesn't work :Container widget; myStructure test;   switch (index) { ...

MMerc.1 by Senior
  • 911 Views
  • 1 replies
  • 0 kudos

Touch Calibration

Hi,Following situation:I have a 480x272 display in portrait mode.(1) In TouchGFXDesigner the 0/0 point is top left with x-axis in horizontal and y-axis vertical down.(2) The expected (by the TouchGFX Framework) touch coordinates are 0/0 top right wit...

jimmii by Senior II
  • 2882 Views
  • 5 replies
  • 0 kudos