STM32 MCUs TouchGFX and GUI

Discuss STM32 and TouchGFX implementations, including configuration, debugging, and optimization.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

X-CUBE-TOUCHGFX 4.26.1 is out!

TouchGFX 4.26.1 is now out. Please follow this link to download it.This version is a patch release and includes bugfixes of issues seen on TouchGFX Designer 4.26.1 version, as well as adding support of the new STM32H5F5 and Chrom-ART 2.Please visit o...

TouchGFX documentation feedback

We wish to always improve our documentation. The best reviews and critics always come from the people that read it, so we would like to use this post to collect your thoughts and feedbacks. Please share what you like, dislike, what you think is missi...

Share your Custom Widgets!

When creating a UI project, you may need widgets that are not part of the TouchGFX library. To create your own graphical element, the TouchGFX team suggests using the Custom Container approach. Since TouchGFX 4.20 it is possible to export and import ...

Freezing when using ARGB8888 dynamic bitmap

The project bitdepth is set in the designer as 16 bit.I need to use a dynamic bitmap to visualise data and, as per a recent suggestion on this forum, I am creating an ARGB8888 format bitmap, however the program freezes, displaying a black area on the...

AndrewM by Associate III
  • 1563 Views
  • 2 replies
  • 0 kudos

USART to TouchGFX

Hi,I use STM32CubeIDE and TouchGFX.Sending to "stm32f746 discovery board" using com port text.When I send different letters, everything is OK.If I send several identical letters, the result is with the character ?example:asdfghjkl -> asdfghjklaaaaaaa...

JNova.0 by Associate III
  • 707 Views
  • 0 replies
  • 0 kudos

Resolved! STM32L151xE and drive lcd

I have used STM32L151xE in a board and drove a glass LCD with it and it works without any problem. But in its datasheet, in two sections, it is mentioned that, STM32L151xE is not support LCD and just STM32L152xE can support it. Is there any explanati...

Sbagh.2 by Associate
  • 1678 Views
  • 2 replies
  • 0 kudos

Touch GFX dynamic Graph widget crash the application

Hello Touch GFX Guys.Hardware: STM32H7B3I development boardSoftware: Touch GFX designer 4.16STM Cube IDE 1.5.0We are trying to experiment with "dynamic graph" widget and experiencing some problems .After adding widget on the screen follow code is ge...

IB.1 by Associate III
  • 9780 Views
  • 20 replies
  • 0 kudos

Resolved! Change from DSI interface to RGB parallel interface

Thank you for helping.environment:MCU: STM32F769BIBoard: CustomSTM32CubeIDE Ver1.5.0TouchGFX Ver4.15.0Import the project created using the STM32F769I-DISCO template with TouchGFX with STM32CubeIDE,After setting the LCD clock with GUII disabled DSI in...

Ebun.1 by Senior
  • 8999 Views
  • 16 replies
  • 0 kudos

Resolved! TouchGFX project with custom board

Hi, I will use STM32H7B3RI in our final product and its not available in TouchGFX so I need to develop a project with STM32CubeMX. I have STM32H7B3I-DK now and I can create projects and run those on development kit. TouchGFX generates its own STM32Cu...

kb24 by Senior
  • 2331 Views
  • 3 replies
  • 0 kudos